Post Go back to editing

Question about AD8495 connection

Thread Summary

The user is considering replacing the AD595 with the AD8495 for thermocouple break detection. The final answer confirms that the AD8495 should have a resistor (100 kΩ to 1 MΩ) connected between the inverting input (-IN) and GND to function properly. The user is using a single-supply configuration with +Vs = 12V, -Vs = GND, and REF = GND, and currently has +IN connected to GND for evaluation.
AI Generated Content
Category: Hardware
Product Number: AD8495

Hello,

I'm using AD595, but since the product is old and new design is deprecated, so I'm considering AD8495 as a replacement.

I have two questions below.

  (1) Is it possible to change the resistor connection for thermocouple break detection connected between -IN and GND to between +IN and GND?

  (2) Is it possible to remove the resistor (connected between +IN to GND) from the state of (1) above?

The connection between -IN and GND outputs "H" when thermocouple disconnection is detected.

Since my power supply voltage is 12 V and 5V MCU is connected to the load  To avoid outputting "H"=12V to the MCU, AD595 is used with +IN connected to GND.

I'd like to minimize PCB modification, I need to confirm whether the AD8495 can be used by connecting +IN directly to GND in the same way.

Best Regards,

Kazu

  • Hi Kazu,

     

    Thank you for reaching out. To further understand the problem and be able to formulate the correct recommendations, we would like to know more about the intended applications and design parameters.

    Please share the following items:

    • What are the values of the supplies? +Vs (Pin7), -Vs (pin3), REF (pin2) of the AD8495
    • Are you using a single-supply or dual-supply configuration?

     

    If there is an electrical connection through a grounded or exposed tip, the resistor value is large enough that any current from the measurement tip to the ground is minimal, preventing measurement errors.

    Hence, It is always recommended that the thermocouple be connected to the ground through a 100 kΩ to 1 MΩ resistor placed at the amplifier’s negative (inverting) input.

    Lastly, The AD8495 inputs require only one (1) ground connection and should be near the inverting input terminal; additional ground connections can form ground loops and possibly the amplifier can’t read the small TCs signal.

    Regards,

  • Hello,

    Thank you for the reply.

     +Vs = 12V, -Vs=GND, REF=GND, Using single-supply configuration.

    Currently, +IN pin is connected to GND for further evaluation.

    Best Regards,

    Kazu

  • Hi  Thank you for your response, for the part to function properly and be able to meet the specs in the Datasheet; it is recommended to put the inverting input terminal to ground through a resistor (100 kΩ to 1 MΩ).

    Best regards