Post Go back to editing

AD82221 Single Supply Operation

Category: Hardware
Product Number: AD8221

I would like to use the AD8221 with +Vs = 10V and -Vs = 0V.

The AD8221 datasheet has the following statement:

This implies that the configuration I am targetting is valid.

Unfortunately if I try to simulate this in LTSpice, the simulation fails unless I tie -Vs to at least about -2.5V. So is the single supply configuration not actually valid, despite what the datasheet claims?

Thanks,

Eric

  • Minor update -- the simulation runs well so long as I tie -Vs to at least -1V. It also runs (very, very slowly) with Vs = -0.5V.

    So... Is the -Vs more negative than GND just a simulation limitation? Or is the datasheet statement (single supply supported) incorrect?

  • Additional update -- the simulation runs well with +Vs=10V and -Vs tied to ground through a 1p Ohm resistance, but fails if -Vs is tied directly to ground. A 1pico-Ohm resistance is arbitrarily small, so I am happy with these simulation results.

    That being said, it would still be nice for an ADI expert / applications engineer to confirm that the single supply operation is a valid operating condition. It is suggested that it is in the single datasheet statement, however there is no other statements / references to this configuration listed. 

  • Hi Eric,

    Good day! I will be working on this. Please let me get back to you once I have an update.

    Best regards