KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADA4255
Recommended for New Designs
The ADA4255 is a precision programmable gain instrumentation amplifier (PGIA) with integrated bipolar charge pumps. With its integrated charge pumps, the...
Datasheet
ADA4255 on Analog.com
To Analog Devices, Inc.
I am using ADA4255CP-EBZ(SN:2021042305881)and EVAL-SDP-CS1Z(SN:2021032503246)with nice controlabilty.
I confirmed it to work normally for gain control.
Next, I like to control the gain through ACE function based on “win32api” developed by the Visual Studio Community 2022 with C++ excluding “.NET etc”.
Comparing https://wiki.analog.com/resources/tools-software/ace/remotecontrol,
I am very glad of me to get the sample program based on “win32api” and/or C++ instead of Python.
Away from software control, I like to control the gain through pin-header (GPIO0~GPIO7).
Please reply me how to apply the control voltage to each pin-electrode without EVAL-SDP-CS1Z(SN:2021032503246).
I hope you to understand my poor English requests.
Thank you.
Hi nysato,
Apologies for the late response.
Away from software control, I like to control the gain through pin-header (GPIO0~GPIO7).
The gains of ADA4255 cannot be controlled using the GPIOs. You can only control them using the SPI pins - CS, SCLK, SDI, SDO. See image below for the SPI Interface:

To control the SPI interface, please refer to the registers below:



Also kindly take note of the voltage levels of the digital pins:

Regards,
Kristine
Hi nysato,
Apologies for the late response.
Away from software control, I like to control the gain through pin-header (GPIO0~GPIO7).
The gains of ADA4255 cannot be controlled using the GPIOs. You can only control them using the SPI pins - CS, SCLK, SDI, SDO. See image below for the SPI Interface:

To control the SPI interface, please refer to the registers below:



Also kindly take note of the voltage levels of the digital pins:

Regards,
Kristine
Dear Kristine,
Thank you for your answer.
Sorry, still my brain do not catch how to control the gain by pin header without EVAL-SDP-CS1Z.
G3, G2, G1, and G0 in Table 12 correspond to CS, SDI, SDD, and SCLK in the SPI pins, thereby, we can apply the DC bias voltage (no serial control) to their each pin in the SPI pins surrounded by yellow line.
As the begginer question, please explain me how to change the register information by using the combination of DC bias voltage applied to pin header ?
Is it possible that ?
I hope you keep in touch with me continuously.
Warm regards, Naoyuki
Hi Naoyuki,
You need to connect the SPI pins to your microcontroller to connect the gain. ADA4255's gain settings cannot be controlled by connecting the SPI pins to a high/low voltage. For more information on SPI interfaces, you can check out this article - Introduction to SPI Interface. Once you have connected your microcontroller to the SPI pins of the evaluation board, you will now write the desired gain register(you can check this out on my previous answer or from the register summary in the datasheet) from the controller then it will transfer this data and control the amplifier. I would also like to clarify that the G0, G1, G2 and G3 does not correspond to the SPI pins in the yellow box. You can also check out the SPI interface discussion specifically for ADA4255 here.
If you want to use DC bias voltage to control your PGIA gain, logic-programmable InAmps would be the best fit. I'm not quite sure of your other requirements but for instance, I would recommend checking out LTC6373 and AD8250.
Hope this helps!
Kristine