Post Go back to editing

pin control for EVAL-ADA4255

Thread Summary

The user inquired about controlling the gain of the ADA4255CP-EBZ through pin headers (GPIO0–GPIO7) without using EVAL-SDP-CS1Z. The final answer clarified that gain control is only possible via the SPI interface (CS, SCLK, SDI, SDO) and not through DC bias voltage on the GPIO pins. The user was directed to the SPI interface documentation and register settings in the ADA4255 datasheet for further details.
AI Generated Content
Category: Hardware
Product Number: 2021042305869
Software Version: 1.26.3240.1417

To Analog Devices, Inc.

I am using ADA4255CP-EBZ(SN:2021042305881)and EVAL-SDP-CS1Z(SN:2021032503246)with nice controlabilty.

I confirmed it to work normally for gain control.
Next, I like to control the gain through ACE function based on “win32api” developed by the Visual Studio Community 2022 with C++ excluding “.NET etc”.

Comparing https://wiki.analog.com/resources/tools-software/ace/remotecontrol,
I am very glad of me to get the sample program based on “win32api” and/or C++ instead of Python.

Away from software control, I like to control the gain through pin-header (GPIO0~GPIO7).
Please reply me how to apply the control voltage to each pin-electrode without EVAL-SDP-CS1Z(SN:2021032503246).

I hope you to understand my poor English requests.

Thank you.

  • Hi nysato,

    Apologies for the late response. 

    Away from software control, I like to control the gain through pin-header (GPIO0~GPIO7).

    The gains of ADA4255 cannot be controlled using the GPIOs. You can only control them using the SPI pins - CS, SCLK, SDI, SDO. See image below for the SPI Interface:

    To control the SPI interface, please refer to the registers below:

    Also kindly take note of the voltage levels of the digital pins:

    Regards,

    Kristine

  • Dear Kristine,

    Thank you for your answer.
    Sorry, still my brain do not catch how to control the gain by pin header without EVAL-SDP-CS1Z.

    G3, G2, G1, and G0 in Table 12 correspond to CS, SDI, SDD, and SCLK in the SPI pins, thereby, we can apply the DC bias voltage (no serial control) to their each pin in the SPI pins surrounded by yellow line.

    As the begginer question, please explain me how to change the register information by using the combination of DC bias voltage applied to pin header ?

    Is it possible that ?

    I hope you keep in touch with me continuously.

    Warm regards, Naoyuki

  • Hi Naoyuki,

    You need to connect the SPI pins to your microcontroller to connect the gain. ADA4255's gain settings cannot be controlled by connecting the SPI pins to a high/low voltage. For more information on SPI interfaces, you can check out this article - Introduction to SPI Interface. Once you have connected your microcontroller to the SPI pins of the evaluation board, you will now write the desired gain register(you can check this out on my previous answer or from the register summary in the datasheet) from the controller then it will transfer this data and control the amplifier. I would also like to clarify that the G0, G1, G2 and G3 does not correspond to the SPI pins in the yellow box. You can also check out the SPI interface discussion specifically for ADA4255 here.

    If you want to use DC bias voltage to control your PGIA gain, logic-programmable InAmps would be the best fit. I'm not quite sure of your other requirements but for instance, I would recommend checking out LTC6373 and AD8250.

    Hope this helps!

    Kristine