Post Go back to editing

AOP Instrumentation

Category: Software
Product Number: NO

Hello,

I would like to find an instrumentation AOP with a gain of around 1500. This AOP accepts low amplitude signals at the input around 1µV to 320µV. Do you know if there are comparator links to find this kind of component ? I use this component in the audio frequency band (10Hz-20kHz).

With a weak PSRR, LOw noise and the supply voltage is +3.3V and -3.3V. 

Thank for your helps

Regards.

Edit Notes

Additional information
[edited by: 206_RC at 1:05 PM (GMT -4) on 12 Jul 2022]
Parents
  • After looking on the Analog site, I found this link but there are parameters that I do not understand very well :

    https://www.analog.com/en/parametricsearch/11080#/

    Perhaps this parameter helps me to find the minimum input voltage level ?

         

    Thank for your helps.

    Regards

  • Hi ,

    Yes, the input noise voltage AND the "0.1Hz to 10Hz" Vnoise (Vpp) are good parameters to choose for when trying to find a part that can extend the lower detection voltage range to 1uV, as in your case.

    For example, you can use this list sorted for lowest noise:

    Excel file showing these parts:

    XLSX

    I took the lowest noise device in that list (AD8428) and simulated its output noise as shown below. Gain is 2,000V/V. I've filtered the output to 20kHz -3dB Bandwidth using C1:

    In your case, the output noise is a combination of 1/f noise (0.1Hz to 10Hz region) as well as the broadband / flatband noise voltage of 1.3nV/RtHz and simulation shows a RMS value of 591uV_RMS. With 1uV hydrophone input signal and a gain of 2,000V/V, the SNR will be:

    SNR = 20* log (1uV_RMS * 2,000V/V / 591uV_RMS) = 10.6dB

    So, you should be able to decipher that low level of input voltage and stay 10dB above the noise floor.

    Here is the simulation file you can use (Extract All before using):

    AD8428 Hydrophone amp with Filter EZ 7_12_22.zip

    Regards,

    Hooman

  • Hello Hooman,

    In fact, probably this component may suit me, I'll have +5V and -5V also in my board. But whe did you use this assembly with 2 generators V3 and E1 ?

    Why can't you just use one sine wave generator to do the same thing ? Like this :

    There is certainly the reason but I do not see yet and also my electronic diagram does not work. 

    Another point, I would have liked to find this same component (same technical characteristics) but with a variable gain up to around 5000 (because I don't know exactly the desired gain).

    Thank for your helps.

    Regards 

  • Hi ,

    In fact, probably this component may suit me, I'll have +5V and -5V also in my board. But whe did you use this assembly with 2 generators V3 and E1 ?

    Response: The two generators used in simulation is just to apply a fully differential, ground-referenced input. In your application, your hydrophone plays that role. 

    Why can't you just use one sine wave generator to do the same thing ? Like this :

    Response: What you've shown is different in that V1 has no CM reference. Some simulations have issues with sources which don't have a ground reference. That's why I used "E" to generate an equal and opposite signal at the input which does have a CM reference to ground.

    Another point, I would have liked to find this same component (same technical characteristics) but with a variable gain up to around 5000 (because I don't know exactly the desired gain).

    Response: Other devices except AD8428 in the Excel file I shared with you earlier allow a range of gains, as shown here:

    So, all you need to do is to select those devices which show min / max gain range.

    Regards,

    Hooman

  • Response: The two generators used in simulation is just to apply a fully differential, ground-referenced input. In your application, your hydrophone plays that role. 

    I'm not sure, as you know in my previous answer I had said that there is a built-in preamp in the hydrophone. And I think at the output of a preamp I will only have 2 wires for signal and ground, that why I want to simulate with a sinusoidal generator (as I did with the LT6233 high pass filter). 

    Do you think if I can use this component AD8428 also as an Allen & Key type high pass filter ? So this AD8428 serves 2 roles: Amplify and filter the signal at the same time. 

    Otherwise I will have to amplify the signal (with AD8428) and add another AOP to filter (I don't know for this moment) before entering my ADC.

    Thank you for your helps

    PS : So in first I need to simulate the AD8428 with with a sine generator.

    Regards

  • Hi ,

    I don't know of a way to make AD8428 operate in Sallen Key low pass filter configuration. I think it's best if you stick with a gain stage and then add the active filter if you need it further in the signal chain.

    You can use your single-ended hydrophone transducer output on AD8428 applied to the +IN pin. You'd then ground the unused -IN pin.

    Regards,

    Hooman

  • You can use your single-ended hydrophone transducer output on AD8428 applied to the +IN pin. You'd then ground the unused -IN pin.

    Hello Hooman,

    Please (read my posts), I d'ont connect the hydrophone directly to the AD8428 because the Hydrophone has a built-in preamp. Thus I connect directely the preampli to the ampli AD8428. But you're right about the electronic connection : the output from the preamp to the amp AD8428 (+IN pin) and to the ground -IN pin (AD8428).

    Do you know Where (the link) I can find the AOP used for a high pass filter with a gain of 1 (Sallen & Key) ? Of course with a very small offset (Ibias).

    Thank you for your helps

    Regards 

  • Hi,

    This is what I get with the simulation with AD8428

    I have always a offset about -50 mV (which is a lot for a component with 50nA Ibias). Probably my simulation is not correct ? Do you have a idea for this simulation ?

    Thank you

    Please see in this attached the simulation

     AD8428_Y.asc   

  • Hi,

    I don't know if this is the right method but I find an output that has very little offset :

    I've just modify the input resistor and

    follow with another AOP to simulate a load. But in principle the gain is 2000 but the account is not there.

  • Hi ,

    With the configuration you've shown (R2 equal to15.11 ohm across the FIL terminals), you've reduced the AD8428 gain (Vout / diff_input) significantly to about 5V/V according to LTspice simulation. I just wanted to point that out to you.

    Regards,

    Hooman

  • Hi Hooman,

    With a Ibias 50n, I have also a offset ? Without R2 I have -50mV (It's very important). what is the simulation assembly that allows not to have an offset and a gain of 2000? Since you advised me this AOP to have no offset (or very low) ? you advised me this AOP according to my constraints it seems to me not ?

    Thank you for your helps.

    Regards

  • Hi ,

    With a Ibias 50n, I have also a offset ? Without R2 I have -50mV (It's very important). what is the simulation assembly that allows not to have an offset and a gain of 2000? Since you advised me this AOP to have no offset (or very low) ? you advised me this AOP according to my constraints it seems to me not ?

    Response: AD8428 has up to 25uV input referred offset voltage (Vos) for the B-Grade (A-Grade Vos is higher at 100uV). The LTspice model has the 25uV built-in. I've cancelled this by adding V_offset to show this below (for demonstration only):

    Here is the simulation file:

    AD8428 Hydrophone amp with Filter EZ 7_20_22.asc

    In your application, you could add a variable offset voltage (+/- 250mV) to the REF pin to compensate for this Vos offset voltage.

    Simulation file:

    AD8428 Hydrophone amp with Filter offset on REF pin EZ 7_20_22.asc

    Regards,

    Hooman

Reply Children
  • AD8428 has up to 25uV input referred offset voltage (Vos) for the B-Grade (A-Grade Vos is higher at 100uV).

     

    For the same component I'll have 2 values, is it an operating range for the same component ?  Or I can choose a component with grade B only ?

    Why I can't take only a generator to simulate the signal as my method (the signal from the first AOP) like this :

    In your simulation, in reality I do not have this connection. Indeed my signal comes from the first preamp and not from the Hydrophone. But why you take this methode to simulate a sine generator ?

    Is it the same as my diagram above ? Thank you for your answer

  • In your application, you could add a variable offset voltage (+/- 250mV) to the REF pin to compensate for this Vos offset voltage.

    Yes, this corresponds more to reality but how to have a circuit with a variable offset (with precision) ? Voltage divider bridge with precision resistors ?

    I'll try this methode with my sinus generator. 

    Another point is after your simulation the gain is not 2000 rather 3650. Why we can have more than a value greater than specified by the constructor ?

  • Hi,

    With this electronic assembly, I'll have the good output signal 

    But the gain is 1400 (It's correct not exactely 2000 as the DS). Probablement it'll be the capacitor 1.3nF ? 

  • Hi ,

    For the same component I'll have 2 values, is it an operating range for the same component ?  Or I can choose a component with grade B only ?

    Response: You can either purchase the A grade (100uV Vos) or the B grade (25uV Vos).

    n your simulation, in reality I do not have this connection. Indeed my signal comes from the first preamp and not from the Hydrophone. But why you take this methode to simulate a sine generator ?

    Response: As I explained earlier in another post (forgot now since we've been communicating so long), the E that I use in LTspice creates the diff input. If you have a single-ended preamp output, then you just use it on IN+ and you can ground IN- (or vice versa), as you've shown it. That'd be fine.

    Regards,

    Hooman