Are the outputs (OUT and ADC_OUT) of AD8293G80B/G160B internally buffered? In other words, can I connect either output directly to my ADC input or do I still need external buffer between my amplifier and ADC to lower the input impedance?
Are the outputs (OUT and ADC_OUT) of AD8293G80B/G160B internally buffered? In other words, can I connect either output directly to my ADC input or do I still need external buffer between my amplifier and ADC to lower the input impedance?
Hi adcl,
Thank you for posting this question.
I will work on this and let me get back to you once I have the information.
Best regards,
Franz
Hi adcl,
Generally speaking, inamps have low-impedance output. However, in this case, ADC OUT (pin 4) has a 5kohm internal resistance used to simplify anti-aliasing filter. If you are going to use the ADC…
Hi,
I think this statement from the datasheet can be the answer to your question: 'Two outputs are available to the user: OUT (Pin 6) and ADC OUT (Pin 4). The difference between the two is the inclusion of a series 5 kΩ resistor at ADC OUT'. So one has 5k output resistence. It depends on your ADC and requirements, if it is suitable for your application.
Hi,
I think this statement from the datasheet can be the answer to your question: 'Two outputs are available to the user: OUT (Pin 6) and ADC OUT (Pin 4). The difference between the two is the inclusion of a series 5 kΩ resistor at ADC OUT'. So one has 5k output resistence. It depends on your ADC and requirements, if it is suitable for your application.