Post Go back to editing

Is the output of AD8293G80B/G160B internal buffered?

Category: Hardware
Product Number: AD8293G80B
Software Version: n/a

Are the outputs (OUT and ADC_OUT) of AD8293G80B/G160B internally buffered? In other words, can I connect either output directly to my ADC input or do I still need external buffer between my amplifier and ADC to lower the input impedance?

  • Hi adcl,

    Thank you for posting this question.

    I will work on this and let me get back to you once I have the information.

    Best regards,

    Franz

  • Yes please.  It's important to know if we can lower component counts to drive ADC input directly from AD8293.  Looking forward to your feedback. Thank you.

  • Hi,

    I think this statement from the datasheet can be the answer to your question: 'Two outputs are available to the user: OUT (Pin 6) and ADC OUT (Pin 4). The difference between the two is the inclusion of a series 5 kΩ resistor at ADC OUT'. So one has 5k output resistence. It depends on your ADC and requirements, if it is suitable for your application.

  • Hi adcl,

    Generally speaking, inamps have low-impedance output. However, in this case, ADC OUT (pin 4) has a 5kohm internal resistance used to simplify anti-aliasing filter. If you are going to use the ADC OUT, you may need to check the allowable RC of the ADC that you will be using.

    Another option for you is to use the OUT (pin 6) if you need a low-impedance connection for the input of the ADC.

    Also, you may want to check the ADC that you will be using. There are some ADCs that has internal buffer at the input.

    Best regards,

    Franz