Post Go back to editing

AD623 input signal offset compensation

I am using an AD623 with a MC33161 voltage monitor to monitor the temperature of a part.

V_SET is around 1.1 V, V_ACT the current temperature monitor voltage being equal to V_SET when the temperature is reached.

Reference voltage for the AD623 is 2.54V from the MC33161. Gain ist set to 213 by R1.
The circuit works well, but some temperature controllers show a difference of up to 6 mV for (V_ACT - V_SET) at stable temperature which is too much for the gain,
an out of valid temperature is indicated by the MC33161 for such an 'offset'.

Hence a compensation of one of the input voltages is needed, which has to be positive or negative, in the range +- 0 to 6 mV.

There is no negative voltage available in the circuit.
A single simple voltage divider at V_SET or V_ACT may not work due the positive as well as negative offset.

Will an OpAmp be the solution to add / subtract a few mV offset or what else can be a stable solution?

Thanks for any hints!!! 

Parents
  • Hi stoccarda,

    Good day and thank you for reaching out to us about your query.
    If I understood correctly the one giving the offset of 6mV are the temperature controllers  which is connected to V_ACT and 'false' triggering the voltage monitor MC33161D because this is being gained up by the inamp. I just want to make sure that all the AD623 works expectedly and I understand the scenario.

    If this is the case will it be okay if you show us the circuitry that connects to V_ACT? This may show us what's causing the offset or if it is inherent with the device/s connected there. The only way I could think off for now is if we can calibrate the effect of the 6mV offset at the output of the AD623 going in to the voltage monitor but this will require doing it for all the temperature controllers.
    Let's see first what we have on the initial stage stoccarda then we'll go from there.
    Thank you.

    Best Regards,
    Dann

  • Hi Dann,

    will you need any more information?

Reply Children
No Data