Customized SPICE Model for AD8421BRZ

HI Sijo,

I got SPICE Model for AD8421(AD8421.cir) from AD website.

But this AD8421.cir model has different VOSI & VOSO values, it is not matching with AD8421BRZ(VOSI=25uV & VOSO=250uV) parameters as per datasheet. 

Could you please provide customized SPICE model for AD8421BRZ, it should include all the parameters(VOSI, VOSO,  etc..) as per the AD8421BRZ datasheet values.

It is urgent requirement, please provide ASAP.

regards,

Tatarao K

9059058519

Parents
  • 0
    •  Analog Employees 
    on Jan 29, 2021 11:01 AM

    Hi Tatarao K,

    Please see attached modified spice model to reflect the B-grade performance of AD8421, particularly on the input offset, output offset, input bias current, and input offset current.

    May I know what applications you are getting into?

    AD8421.zip

    Best regards,

    Emman

  • HI Emman,

    We are using this AD8421BRZ op amp for Current sense measurement with gain 80, and bandwidth is MHz.

    I have few queries regarding New Model AD8421BRZ which you shared with us,

    1. Temperatures effects not modeled, that means which temperature this model will support?.

    BEGIN Notes:
    *
    * Not Modeled:

         * Temperature effects
         * PSRR

    2. As per the AD8421BRZ datasheet, VOSO is 250uV, but this model has -1.75mV( VOSO VOUT N015 -1.75e-3).

    Which one is correct?. this AD8421BRZ model or datasheet values?.

    regards,

    Tatarao K

  • 0
    •  Analog Employees 
    on Feb 3, 2021 12:58 PM in reply to ktr

    Hi Tatarao K,

    The model only supports ambient temperature at 25°C.

    The netlist compensates other factors inside the spice model but if you will going to measure the actual output offset voltage of the updated model, you'll see that it is around 250uV. 

    Best regards,

    Emman 

  • HI Emman,

    Thanks for clarification, my understand is this updated model netlist showing VOSO= -1.75e-3, but this model contains 250uV, right?.

    Another query is, 

    I am doing 2layer PCB layout, shall i keep Gain resistor of AD8421BERZ at Bottom layer?. since i am routing input signal as differential, no place available at TOP side.

    regards,

    Tatarao K

Reply
  • HI Emman,

    Thanks for clarification, my understand is this updated model netlist showing VOSO= -1.75e-3, but this model contains 250uV, right?.

    Another query is, 

    I am doing 2layer PCB layout, shall i keep Gain resistor of AD8421BERZ at Bottom layer?. since i am routing input signal as differential, no place available at TOP side.

    regards,

    Tatarao K

Children