Post Go back to editing

Instrumentation Amplifier Gain resistor(s)

Hi. I am looking for Instrumentation Amplifiers for an application.  At this stage, we have decided a certain gain value for our Instrumentation Amplifier. The datasheet of the product mention the very precise value of gain resistors to attain certain gain value.

We haven't ordered the products yet as I am confused about whether we will be able to acquire the gain resistors ourselves (from some other manufactures) or they will come with the Instrumentation Amplifier package we will order?  Because these gain resistor values for certain gain sets are very precise which are difficult to get from manufactures. I am attaching the screenshot of AD8237 gain resistors from datasheet as reference  https://www.analog.com/media/en/technical-documentation/data-sheets/AD8237.pdf

Parents
  • DB,

      You will find that the majority of error, especially over temperature, usually comes from the resistors.

    You can go to Digikey.com and buy 5%, 2%, 1%, 0.1% resistors, etc. with tempcos of 50 ppm, 25 ppm, etc.

    but the best thing is to use a monolithic resistor array so the the resistors track over temperature.

    such as the LT5400-xx

    Harry

Reply
  • DB,

      You will find that the majority of error, especially over temperature, usually comes from the resistors.

    You can go to Digikey.com and buy 5%, 2%, 1%, 0.1% resistors, etc. with tempcos of 50 ppm, 25 ppm, etc.

    but the best thing is to use a monolithic resistor array so the the resistors track over temperature.

    such as the LT5400-xx

    Harry

Children
No Data