AD624

Is there any instrumentation amplifier which has same spec or better to AD624 (mil grade) but with SMT packaging?

  • renj,

      There are over 15 specs in the spec table.  When you say "same spec or better...", which one(s)

    are important to you?

    Does it have to run on +/-15V, +/-5V, ground and 3.3V??

    Is 1 MHz required or would 10 kHz be o.k.?

    Is supply current critical?

    Does it have to be pin strapped or would digital programming from a microprocessor work?

    Etc.

    You need to give us more detail about what you need.

    Harry

  • 0
    •  Analog Employees 
    on Aug 2, 2018 2:34 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin