Post Go back to editing

AD8220 output voltage swing as a function of Vs & Rg

Thread Summary

The user is troubleshooting the AD8220 instrumentation amplifier to measure resistance tolerance. The issue is due to operating outside the valid input voltage range (3V for 5V supply). Removing the 1kΩ resistor or increasing the supply voltage to 8V resolves the problem. The input common mode range is also a potential limitation.
AI Generated Content

I'm trying to use the AD8220 to measure resistance tolerance, here is my circuit and measurements :

Could you please advise  the difference in output voltage swing, as a function of: (V+- V-),VS & Rg ?

Thanks

Parents
  • Hi mosnu,

    For the 5V operation, it looks like you are operating outside of the valid input voltage range of the amplifier. From page 6 of the datasheet, the valid input voltage range of the AD8220 only allows input voltages from -0.1 to 3V (for the case of a 5V supply). Looking at your circuit, if you have a 2mA current running through your resistors, Vin+ would already be seeing 4V, resulting in an invalid output. When you extend the supply to 8V, the input voltage range now goes to 6V, which is why you get the correct output at the AD8220.

    Is the lower 1k resistor needed? Your circuit will work at 5V if you remove this since the voltage at the input pins will sit within the input voltage range of the part.

    I hope this helps!

    Kris

Reply
  • Hi mosnu,

    For the 5V operation, it looks like you are operating outside of the valid input voltage range of the amplifier. From page 6 of the datasheet, the valid input voltage range of the AD8220 only allows input voltages from -0.1 to 3V (for the case of a 5V supply). Looking at your circuit, if you have a 2mA current running through your resistors, Vin+ would already be seeing 4V, resulting in an invalid output. When you extend the supply to 8V, the input voltage range now goes to 6V, which is why you get the correct output at the AD8220.

    Is the lower 1k resistor needed? Your circuit will work at 5V if you remove this since the voltage at the input pins will sit within the input voltage range of the part.

    I hope this helps!

    Kris

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.