Post Go back to editing

AD8220 output voltage swing as a function of Vs & Rg

Thread Summary

The user is troubleshooting the AD8220 instrumentation amplifier to measure resistance tolerance. The issue is due to operating outside the valid input voltage range (3V for 5V supply). Removing the 1kΩ resistor or increasing the supply voltage to 8V resolves the problem. The input common mode range is also a potential limitation.
AI Generated Content

I'm trying to use the AD8220 to measure resistance tolerance, here is my circuit and measurements :

Could you please advise  the difference in output voltage swing, as a function of: (V+- V-),VS & Rg ?

Thanks

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.