Post Go back to editing

AD8220 output voltage swing as a function of Vs & Rg

Thread Summary

The user is troubleshooting the AD8220 instrumentation amplifier to measure resistance tolerance. The issue is due to operating outside the valid input voltage range (3V for 5V supply). Removing the 1kΩ resistor or increasing the supply voltage to 8V resolves the problem. The input common mode range is also a potential limitation.
AI Generated Content

I'm trying to use the AD8220 to measure resistance tolerance, here is my circuit and measurements :

Could you please advise  the difference in output voltage swing, as a function of: (V+- V-),VS & Rg ?

Thanks

  • Hi mosnu,

    I am looking into this. I'll get back to you soon.

    Thanks!

    Kris

  • Hi mosnu,

    For the 5V operation, it looks like you are operating outside of the valid input voltage range of the amplifier. From page 6 of the datasheet, the valid input voltage range of the AD8220 only allows input voltages from -0.1 to 3V (for the case of a 5V supply). Looking at your circuit, if you have a 2mA current running through your resistors, Vin+ would already be seeing 4V, resulting in an invalid output. When you extend the supply to 8V, the input voltage range now goes to 6V, which is why you get the correct output at the AD8220.

    Is the lower 1k resistor needed? Your circuit will work at 5V if you remove this since the voltage at the input pins will sit within the input voltage range of the part.

    I hope this helps!

    Kris

  • Hi Kris,

    Thanks for your quick and helpful answer.

    But in that case (that my input voltage getting closer to (Vs-2V=3V) Shouldn't I get the Max. Rail voltage on Vout ?

    (as saturated amp )

    Thanks



  • Hi mosnu,

    Not necessarily. Operating outside of the input voltage range puts you in an undefined state so your results may be unpredictable. However, I think that in your case, you may also be hitting some limitations due to your input common mode range. You can check this thread for more information.

    I hope this helps!

    Kris

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.