AD620 drift

Hi,

I use ad620 for my load cell conditioning circuit. It amplifies load cell signal to +/- 10V range. I need to improve drift cause by temperature. When I apply just a little hot air to my pcb and output changes.

I have ad620 with a gain of 660. I have +10V and -10V regulated from +/-15V. I use reference pin of ad620 in order to remove dead weight. because after ad620 I further amplify my signal with a gain of 12. then a low pass filter. My filter is around 3Hz.

I use 10ppm thin film resistor on gain adjustment and 25ppm in my filter and voltage regulator circuits.

does any one has an idea on getting better temperature performance.

Parents
No Data
Reply Children
No Data