AD8251, AD8253 Model Convergence

Hi,

I am attempting to use the AD825x devices as current sense and voltage sense instrumentation amplifiers in an analog control loop. I was unable to get the SPICE models for the AD825x to work with PSpice and LTSpice. While the circuit simulation was stable with an approximation of the AD825x (gain followed by a low pass filter), the actual circuit when built was not stable.

I understand that my approximation of the gain/phase response of the instrumentation amplifier was not detailed enough, the frequency response of the devices is critical to the stability of the circuit.

I need some help getting a basic circuit to converge with the actual devices. I have built a simple model below; however this model does not converge.

I get the following error (The full SPICE output is attached):

  These supply currents failed to converge:

    I(X_U1.EREF1)             =   -10.00GA  \   -10.00GA

    I(X_U1.EPSB1)             =   -10.00GA  \   -10.00GA

The basic idea of the application is shown below:

Any help would be appreciated. Thanks!

Igor

Trans.out.zip
Parents
  • Hi Guys,

    Thanks for your help. I re-made the parts and the simulation works (although it still does not converge every time.)

    My simulation is currently is shown below. For some reason I am seeing input bias currents of about 4uA (top plot) into U1. This seems a little high to me. It is producing an offset of a few mA due to the high input resistances (2nd plot from the top).

    Is this a simulation artifact? How can I improve the input currents? I tired running the AD8251 from +/- 15V with similar results. The datasheet quotes input currents in the order of 50nA.

    Thanks!

Reply
  • Hi Guys,

    Thanks for your help. I re-made the parts and the simulation works (although it still does not converge every time.)

    My simulation is currently is shown below. For some reason I am seeing input bias currents of about 4uA (top plot) into U1. This seems a little high to me. It is producing an offset of a few mA due to the high input resistances (2nd plot from the top).

    Is this a simulation artifact? How can I improve the input currents? I tired running the AD8251 from +/- 15V with similar results. The datasheet quotes input currents in the order of 50nA.

    Thanks!

Children
No Data