Measuring multiple current ranges simultaneously

Dear Fellows,

     We have a task to measure a current range from 1uA to 300mA. The measurements must be completed without switching the range with a BW of 250kHz.

     The proposed solution is:

  • Use of a 10 ohm shunt resistor
  • For high range use a high gain instrumentation amplifier AD8428 with the gain set to 300 and and offset voltage compensation connected to the REF pin by the aid of an OP177
  • For low range AD8421 with the gain set to 1

     Question:

     I see a big risk of overloading the high gain instrumentation Opamp thus, leading to saturation of it's output stage. How can be avoided this?


     Could it help if we use one amplifier the AD8428 and to have two switched trimmers set to 3R for 1x and 1058R for 300x gain?

     I would switch between two gains with two Opto-Mosfets driven by a fast comparator connected to the instrumentation amplifier's output.

     Some other data:

     Full scale voltage is 3.000V (Vref)

     ADC used is 12 bits internal uC SAR ADC.


Any advice is highly appreciated, thank you, Endre

  • 0
    •  Analog Employees 
    on Apr 12, 2016 12:01 AM over 4 years ago

    Hello Endre,

    I apologize for the late reply. Have you considered using a programmable gain instrumentation amplifier like the AD8253? Basically, you could use a single sense resistor of 10ohms like you say, and just switch gains depending on what range of current you are measuring. If the bandwidth you require is 250kHz, you can go up to a gain of 100. I think the ADC would still be able to resolve this.

    Could you provide more details about your application? What are you taking current measurements on?

    Thanks,

    Kris

  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:23 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin