Hi
AD8039 can work with a single power supply?
According to its data sheet, the supply range is 3V to 12V but my AD8039 output 1V under 0V input and 5V single power supply condition. It works correctly (output=0V) by changing +/- 5V supply.
Regards,
Kazu
In the spec table, the output is +/-4V when running on +/-5V, so we can deduce that the
output only gets within 1V of either rail. So on ground and +5V, the output should swing
between +1V and +4V.
Note that the input common mode range is also +/-4V when running on +/-5V, so on ground
and +5V, you will have to keep the inputs with a 1V to 4V range.
There is no ground pin on the op amp, so the 3V to 12V spec is telling you that is the voltage
you have to have across the part (from V- pin to V+ pin) to get it to work.
So you could run it on -2V and +5V if you have any unregulated negative voltage from -2V to
-5V.
Harry