Can AD8306 be used as an AGC amplifier

Hello,

   I'm a bit confused about AD8306.Can this chip control the output amplitude?Can it be used as an AGC amplifier?

   Thanks!

Parents
  • Hi,

        I still have a question, if my input range is -62dBm~-1dBm, then zoom in through AD8306, and finally I can enter the AD9430 chip.Is there any problem with such a plan,please?I saw the chip datasheet that the maximum output voltage in LIMTING AMPLIFIER  is 1.25V. Does it mean hat by setting when my input is -1dBm, my output can reach 1.25V(11.94dBm)? 

       I hope to get your reply as soon as possible.Thanks very much!

Reply
  • Hi,

        I still have a question, if my input range is -62dBm~-1dBm, then zoom in through AD8306, and finally I can enter the AD9430 chip.Is there any problem with such a plan,please?I saw the chip datasheet that the maximum output voltage in LIMTING AMPLIFIER  is 1.25V. Does it mean hat by setting when my input is -1dBm, my output can reach 1.25V(11.94dBm)? 

       I hope to get your reply as soon as possible.Thanks very much!

Children
No Data