Post Go back to editing

AD8000/AD8009 Power supply

Hi,

Can these amplifiers be powered from a single +12V power supply. The datasheet only shows +/-5 V and 5V; however the max. power supply is set to +12.6 V in the datasheet.

Or, when operation between +/- 5V is only feasible, can I use a RF transformer at the output to have 0-10V signal swing (I want to use the devices as a pulse amplifier into 50 ohm coax with source and end termination with 5V levels at the load; pulses can be as short as 10 ns).

Thanks for your help,

Best regards