Post Go back to editing

AD8479

Hi there,

What is the maximum input differential voltage range of AD8479 when operating at a single power supply of +5V ? Is it +-4.7V? 

If it is, what is the allowed input differential voltage range that can his device survive(both continuous and pulse conditions) at a single power supply of +5V? Absolute maximum specification mentions about common mode voltage but no differential input voltage. 



TYPO
[edited by: tae213 at 4:55 AM (GMT -4) on 26 Jun 2023]

Top Replies

    •  Analog Employees 
    in reply to tae213 +1 verified

    Hi  ,

    The datasheet only specifies the +/-15V supply with 14.7V differential voltage but it is also expected to scale on different supply voltages so we can expect +4.7V max differential on a single…

Parents Reply Children
No Data