Hi,
I am not an expert in RF; I am trying to design a signal power meter for satellite application using AD8307 log Amp.
Below is the schematic that uses BPF (BPF-C70+) to filter unwanted signals and to allow only 70MHz signals. I am able to see the 70Mhz RF signal in spectrum but the voltage measured at output of AD8307 is not as per calculated value 25mv/db.
Please let me know where I am doing wrong.
Below are the different cases we observed while testing:
Case 1: (20dB input/fc:70MHz) consider filter Insertion Loss at 70MHz is 6.4dB the input to AD8307 is 13.6dB
- Input Signal to BPF: Signal Absolute Level = -82.3dbm / Noise Floor = -102.3
- Output: Voltage at Pin 4 of AD8307 is 0.51V without signal 0.48V (just at Noise floor level)
Case 2: (22dB input/fc:70MHz) consider filter Insertion Loss at 70MHz is 6.4dB the input to AD8307 is 15.6dB
- Input Signal to BPF: Signal Absolute Level = -36.3dbm / Noise Floor = -58.3
- Output: Voltage at Pin 4 of AD8307 is 1.45V without signal 1.41V (just at Noise floor level)
Case 3: (25dB input/fc:70MHz) consider filter Insertion Loss at 70MHz is 6.4dB the input to AD8307 is 18.6dB
- Input Signal to BPF: Signal Absolute Level = -61.3dbm / Noise Floor = -86.3
- Output: Voltage at Pin 4 of AD8307 is 1.05V / without signal 1.04V (just at Noise floor level)
I also tested the same circuit by just replacing BPF (F455K000S011) with 455Khz one. below are the results observed.
BPF specification: Bandwidth (+/- kHz) 3 kHz, Insertion Loss 6 dB, Input/Output Impedance (Ohms) 2000 Ohms.
- Input Signal to BPF: Signal Absolute Level = -27.3dbm / Noise Floor = -56.3
- Output Observed on Pin-4 of AD8307 is ranging from 1.834V to 2.136V and difference is 302mV. Ideally, I am expecting 25dB/V x 29dB = 725mV as per the datasheet.
Added input signal details to the 455khz filter configuration.
[edited by: ANURAG at 7:50 PM (GMT -4) on 25 May 2021]