Post Go back to editing

Instability of the output signal ADA4522-2

Hi! I'm using the ADA4522-2 as a differential op-amp. According to the tests and simulation results in LTspice, the output differential voltage is approximately 24V. If you use a different operational amplifier, for example, OP2177, this problem disappears and the voltage is 2.5 V. There is an ideal 20 mA differential current source at the input of the circuit.

Can you tell me what the problem may be and how to fix it?

Figure 1 - Differential output voltage OP2177

Figure 2 - Differential output voltage ADA4522-2



Signed figure 2
[edited by: Vladimirovich at 1:09 PM (GMT -4) on 18 May 2021]
Parents Reply Children
No Data