AD8495 attached K type thermocouple

Hi,

I am using a AD8495 amplifier which is attached to the  K-type thermocouple to amplify the thermocouple output voltage. I supplied 10.0 V to the amplifier by using an external power supply unit. My temperature measuring range is 0 0C to 150 0C. Output voltage values have already been  measured  and collected into the Excel sheet. So, I need to convert (Voltage values) them into Celsius. Can I do it by using any simply equation?  OR

Should I write MATLAB or Python scripts in order to convert these voltage values into Celsius?

I am much grateful if you can help and guide me to do that.

Many Thanks & Best Regards,

Niroshan



tag
[edited by: lallison at 9:44 PM (GMT -5) on 15 Jan 2021]