Hi,
I need some help.
As below picture picked from the datasheet. it said EPAD can connect to V- or leave floating, does ADA4666-2 also work if connected EPAD to GND?
I mistakenly connected EPAD and GND, it sees the consumption of current rised.
I will make a change in the next design, and want to know what is the potential risk in my current circuit.
Best Regards,Leo
It could possibly cause undesired running currents through the die in undesired and destructive paths.
Hi Leo,
On your circuit, where did you connect your V-? Is it shorted to GND?
Highly recommended is connect EPAD to V-.
The power condition of my circuit is below.
V+ is +3.3V,
V- is -7.5V
Does the IC get damage when connecting EPAD with GND?
Thanks,