using an ADA4522 (dual pack) for a buffer/inverter setup. so, one of theamps setup as typical volt follower, the other a inverting amp. BOth are driven from an AD8221.
The AD8221 is outputting a 20KHz sine biased at 2V. Vpp on sine = 2V...
When I sweep the freq up to about >190KHz...somehwere in there, the volt follower section appears to slew/clamp, oscillate...while the inverting side looks fine.
+-12V dual supplies on chip. Tried inserting a 332ohm in series with the volt follower input..didnt do anything...tried removing DC bias...did nothing....not driving capacitive load.
just looking for the reason this might be happening....???
jwyounghster@verizon.net