On the Wafer layout of AD630SD/883B products

Dear Support

Why is the layout of the PN:AD630SD/883B DC:2019+ wafer different from that of the datastheet when we order it?

This is the layout on the datasheet in the specification.

This is AD630SD/883 DC:2019+ by de-encapsulating the components, and the wafer layout can be seen visually as shown in the figure:
(for example, a microscope with a magnification of 200X) de-encapsulate the assembly

As shown in the picture, the red mark is different from datasheet.


I would like to ask, why is the layout of the wafer different from that of the datasheet?


Does ADI have any information on this?


Can you provide me with the latest wafer layout?


Thank you very much.

Parents Reply
  • +1
    •  Analog Employees 
    on Jun 16, 2020 4:28 PM 10 months ago in reply to lerry

    Hi Lerry,

    The attached PDF is the MIL version of the AD630 datasheet.  It involves a documentation change.  It also applies to packaged parts.  You are packaging bare die into your own package, if I understand correctly.

    AD630SCHIPS is the die only part number.   PCN# 07-0092 from Mar/2008 is the last change (100mm to 150mm wafer).

    So there has not been any changes to the die since 2008.

    Cheers,

    George

Children