I would like to use the SSM2143 Differential Line Receiver in a Dual Channel Audio Interface and A/D Converter, but the available supply voltages are lower than the +/- 15 V indicated by the datasheet.
I would be very grateful if somebody could tell me what are the performances (max. Input Level, Distortion, Noise) of the device when powered with +/- 10 V, considering an output load between 2 and 10 kOhm, and a -6dB Gain configuration.
Thank you very much in advance!
Alberto