Post Go back to editing

ADA4000 comparator

Hi AD,

is the ADA4000-1 can be used as a comparator instead of amplifier and is it a dedicated op-amp to work for this kind of use (e.g comparator)

It seems that ADA4000 is highly sensitive working as a comparator and it doesn't like this non linear mode.

Moreover with a transistor on the output which could create high DV/DT for example.

thanks for your help,

Parents
  • Hi,

    Its it possible that there are a few sources of failure here. You did mention that the output actually rails to the maximum value it can on the low-side. This would tell me that it isn't a fault on the output, such as an ESD diode fusing to the low side supply due to an over-stress condition.

    I have some questions:

    If you take your input and ground it, what does your output read?

    What are the values of resistors you are using for your gain of -2?

    For a gain of -2, with 0-20V in, you would output 0 to -40V. As your supply on the negative side is limited to -15V, I would expect anything beyond +7V to rail the device. Once you go about 7V in, I would then expect the inverting terminal to follow (at an offset) the input: At 8V in, with Vout = -14, your inverting terminal would read about 0.66V. At 9V, the inverting node would go to about 1.333V, and continue to increase proportionately at 2/3V per V of Vin. When you continue to exceed the compliance of the device, you may be observing phase inversion of the part.

    Really, without a schematic it is very difficult to debug the circuit. What I then would recommend is to look at our op-amp text book for more information: http://www.analog.com/library/analogDialogue/archives/39-05/op_amp_applications_handbook.html

    Cheers,

    -David

Reply
  • Hi,

    Its it possible that there are a few sources of failure here. You did mention that the output actually rails to the maximum value it can on the low-side. This would tell me that it isn't a fault on the output, such as an ESD diode fusing to the low side supply due to an over-stress condition.

    I have some questions:

    If you take your input and ground it, what does your output read?

    What are the values of resistors you are using for your gain of -2?

    For a gain of -2, with 0-20V in, you would output 0 to -40V. As your supply on the negative side is limited to -15V, I would expect anything beyond +7V to rail the device. Once you go about 7V in, I would then expect the inverting terminal to follow (at an offset) the input: At 8V in, with Vout = -14, your inverting terminal would read about 0.66V. At 9V, the inverting node would go to about 1.333V, and continue to increase proportionately at 2/3V per V of Vin. When you continue to exceed the compliance of the device, you may be observing phase inversion of the part.

    Really, without a schematic it is very difficult to debug the circuit. What I then would recommend is to look at our op-amp text book for more information: http://www.analog.com/library/analogDialogue/archives/39-05/op_amp_applications_handbook.html

    Cheers,

    -David

Children
No Data