Post Go back to editing

ADA4000 comparator

Hi AD,

is the ADA4000-1 can be used as a comparator instead of amplifier and is it a dedicated op-amp to work for this kind of use (e.g comparator)

It seems that ADA4000 is highly sensitive working as a comparator and it doesn't like this non linear mode.

Moreover with a transistor on the output which could create high DV/DT for example.

thanks for your help,

Parents
  • Thx for your help David,

    I understand the black box problem. I will think about it.

    In addition, and in order to find the root cause of failure, I have tested each op-amp by wiring them as an inverting circuit (Gain = -2). I inject a DC voltage source between 0V up to 20V on the inverting input of op-amp (not recommanded regarding the datasheet when op-amp is power supplied by +15V/-15V) and non inverting input is wired to ground.

    2 failure modes are raised.

    - output is always equal to -Vsat (i.e close to -13,7V or -14V) whatever input voltage is between 0V and 20V.

    - output follow the inverting input, as to know the voltage source, and op-amp clamps output voltage to 15,7V or 16V when voltage source is between 15V and 20V.

    I try to find a common failure mode, any idea on what I can do on my black boxes ?

    Additional clue : it is possible that sometimes I have injected a DC voltage source on inverting and non-inverting inputs before powering op-amp on +/-Vcc. Not recommanded too isn't it ?

Reply
  • Thx for your help David,

    I understand the black box problem. I will think about it.

    In addition, and in order to find the root cause of failure, I have tested each op-amp by wiring them as an inverting circuit (Gain = -2). I inject a DC voltage source between 0V up to 20V on the inverting input of op-amp (not recommanded regarding the datasheet when op-amp is power supplied by +15V/-15V) and non inverting input is wired to ground.

    2 failure modes are raised.

    - output is always equal to -Vsat (i.e close to -13,7V or -14V) whatever input voltage is between 0V and 20V.

    - output follow the inverting input, as to know the voltage source, and op-amp clamps output voltage to 15,7V or 16V when voltage source is between 15V and 20V.

    I try to find a common failure mode, any idea on what I can do on my black boxes ?

    Additional clue : it is possible that sometimes I have injected a DC voltage source on inverting and non-inverting inputs before powering op-amp on +/-Vcc. Not recommanded too isn't it ?

Children
No Data