Post Go back to editing

ADA4000 comparator

Hi AD,

is the ADA4000-1 can be used as a comparator instead of amplifier and is it a dedicated op-amp to work for this kind of use (e.g comparator)

It seems that ADA4000 is highly sensitive working as a comparator and it doesn't like this non linear mode.

Moreover with a transistor on the output which could create high DV/DT for example.

thanks for your help,

Parents
  • Hello Jaja,

    We do not necessarily need the full system schematic, but merely the section with the amplifier. Without the schematic, we have no means to understand how the device is being applied and with it, the possible failure modes. One can neither diagnose a malfunctioning black box, nor declare with certainty the root cause if the box cannot be opened or investigated.

    Poor supply decoupling will generally not be a problem as that is a function of PSRR.

    Asymmetric supplies are not a problem, so long as their values do not exceed the absolute max ratings of the part. ESD is a possibility, but again no information is provided about the failure mode to believe it to be ESD with any certainty.

    Cheers,

    -David

Reply
  • Hello Jaja,

    We do not necessarily need the full system schematic, but merely the section with the amplifier. Without the schematic, we have no means to understand how the device is being applied and with it, the possible failure modes. One can neither diagnose a malfunctioning black box, nor declare with certainty the root cause if the box cannot be opened or investigated.

    Poor supply decoupling will generally not be a problem as that is a function of PSRR.

    Asymmetric supplies are not a problem, so long as their values do not exceed the absolute max ratings of the part. ESD is a possibility, but again no information is provided about the failure mode to believe it to be ESD with any certainty.

    Cheers,

    -David

Children
No Data