Post Go back to editing

AD835

hi engineer,

i want to function ad835 as a multiplier. i want to make this component to produce BPSK Signal. i had a discussion with Mr. Neil and he suggested to visit this forum. i have applied the example of design BPSK that used AD835. i have tried it but it didn't work. please help me how to use AD835 to produce BPSK signal. thank you.

Best Regards,

mira_21

example_designBPSK.pdf
  • Hi-

    I have moved this question about the AD835 to the Amplifiers community.  Someone here should be able to assist you.

    Regards,

    AndyR

    EngineerZone Support Community Manager

  • Hi mira_21,

    I replied to your other post. I thought that the DDS community might be able to help you since they have single chip solution that is capable of producing BPSK signals. But apparently, you wanted to go with a discrete BPSK circuit that makes use of the AD835 multiplier IC. Is this correct? Please take a look at  my reply to the other thread.

    Thank you,

    Neil

  • Hi Mr.Neil,

    thank you so much for your attention about my problem. yeah, i wanna make BPSK modulator using AD835 cause i have bought it. here i attach a file about my BPSK circuit. sorry if this circuit looked bad, cause i'm newbie.

    After you look at my circuit, please tell me what is wrong with my circuit cause the output was not producing BPSK signal.

    Thank you,

    Mira_21

  • Hi Mira_21,

    Thank you for clarifying that. I looked at your actual circuit and I noticed that R3 is connected differently as compared to the circuit in the paper you were referring. Have you checked on this?

    Also, I am curious on the signals at the X1 and Y1 pins. Could you take some scope shots on these input pins? I want to make sure that we are having the correct input levels for the AD835. If possible, please include the output bpsk signal on the scope shot.

    Regards,

    Neil

  • Hi,

    There was no scope shots for the inputs on the document the you attached. Could you re-send the scope shots of the two inputs on the same picture?

    On the paper you sent earlier, the oscillator output is connected to the X1 pin via a resistor divider. However, the one you built had a different resistor configuration. I am not sure though if this could affect your circuit as long as the input pins of the AD835 are within the specified voltage range.

    Thanks.

    additional discussion added to reply. Message was edited by: Neil Kane Jacalan

  • Hi Mr.Neil.

    Tq for your respon.

    i attached the input and output of my circuit.

    please tell me what was wrong with my circuit.

    about R3 that i have made, i thought it similiar to the circuit of the paper that i have sent to you. 

    thank you.

    mira_21

  • mr. neil, this is my scope shot of INPUT X1 and Y1. thank you..

  • Hi,

    Thank you for the scope shots. Your inputs seem to be good. However, are the digital signal and carrier signal synchronized? In order to properly implement BPSK, the carrier frequency must be an exact multiple of the digital bit clock such that they cross the zero level at the same time. I can't tell whether your carrier and digital clock are synchronized based on your AD835 schematic and input scope shots. The reason why I asked for the inputs to be on the same scope shot (or the same picture) is to see whether they cross the zero level at the same time.

    Best regards,

    Neil

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin