Post Go back to editing

A couple of questions for AD8336

Dir Sir/Madam,

I have a couple of questions for AD8336 as following.

1)

What is the input-impedance of VGAI pin?

I can see the 1.28kohms on your datasheet page-20.

Does this means the impedamce,correct?

2)

Why is LPF(low pass filter) put at AN-934 page-4?

(closing output pin, 100ohm and 4.7nF)

I think that this means 36kHz cut off frequency.

eg) If I need the 20kHz cut off frequency, can I put the 20kHz LPF there?

3)

If I dont use the internal preamp on AD8336, how can I deal the opened 3 pins INPP, INPN, and PRAO?

In general, connect INPP to GND, and short INPN to PRAO, correct? It is similar as voltage follower circuit.

Thanks, KAOS

Parents Reply Children
No Data