I am using AMP01fx IC for amplifying micro volt signal from the three terminal input. The two terminals are connected to differential
input of AMP01fx and the 3rd terminal input is to be connected to Guard Drive. I need to implement Guard Drive Connection Circuit which is given in the Amp01fx Datasheet(Page no.13, Fig.31).
But in the Fig.31 I am not sure whether i need to implement the dashed connections or the Solder Link Connections in the circuit and if i am not going for Solder link connection what will be values of R3, R4, R5. Please help me in this regard.....