AD8608 driving 600 Ohm Impedance line through isolation transformer

I have searched the internet for hours upon hours to find answers to my questions with no luck... Below are 2 circuits that are a part of a project I am working on.... These are the interface circuits between my system and a balanced signal TDM box with 600 Ohm termination (old school Voice Freq Channel to T1 multiplexer)... The problem is when I run voice grade tests through the system I am getting poor results and I am almost 100% there is impedance mismatch causing the problems. I don't have much experience with telephony interface circuits (or impedance matching between op amps and transformers) and am seeking help....

Figure 1: The input side of the circuit

Figure 2: The output side of the circuit

These circuits were derived from the ADAU1442-EZ board which is the DSP we are using for this application.

On the input side of the circuit a balanced signal comes into the transformer which has a 1:1 ratio.  I have the 680 Ohm resistor to ground but I think I need to put a 2.16uF capacitor in series with that 680 Ohm resistor to match the line impedance, right?

On the output side I think I should remove the 22k Ohm resistor along with the 3.3nF and 4.7uF cap (replacing the 4.7uF cap with a 2.16uF), again to match the line impedance, but I am not 100% about this.

Is this problem a lot bigger than what I think? Part of our circuit also has a built in telephone hybrid (dual transformer design) which when activated bypasses the 1:1 isolation transformers (not shown in the above figures but the op amp circuits are the exact same). That is where I am seeing the worst voice grade test results (with the hybrid in the circuit).

I appreciate any feedback provided.

Parents
  • The intermodulation distortion at a 23-tone test signal of -15 dBm is returning a 3rd order of ~+50 dBm which is 1 dBm above the threshold. We want it to be >+60 dBm. The 2nd order is also low (~+55dBm). That is the main test that I am concerned with. The results seem to fluctuate quite a bit (+/- 5 dBm when we usually see +/- 2 or 3 dBm which I think is a "flanging" effect going on due to the bad impedance matching).

    The board is a 4 layer board with the inner 2 layers being power and ground. I worked on the circuit design but we had a vendor do the actual PCB layout and production (prototypes). The primary frequencies we are interested in are 304 Hz to 3004 Hz at -13 dBm with the exception of the 23-tone test.

    As for the test setup we are running a TIMS test set to a 66 block which connects to the card/cage via 60 pin telco cable. We've never quantified our circuits by THD before, but maybe I should look into it...

    On the card itself after passing through the op-amp circuits it goes to a AD1938 codec and to the ADAU1442 for processing.

    Could the internal filters of the DSP be causing the bad harmonics in the Intermod distortion test?

    Thanks for responding to my post.

Reply
  • The intermodulation distortion at a 23-tone test signal of -15 dBm is returning a 3rd order of ~+50 dBm which is 1 dBm above the threshold. We want it to be >+60 dBm. The 2nd order is also low (~+55dBm). That is the main test that I am concerned with. The results seem to fluctuate quite a bit (+/- 5 dBm when we usually see +/- 2 or 3 dBm which I think is a "flanging" effect going on due to the bad impedance matching).

    The board is a 4 layer board with the inner 2 layers being power and ground. I worked on the circuit design but we had a vendor do the actual PCB layout and production (prototypes). The primary frequencies we are interested in are 304 Hz to 3004 Hz at -13 dBm with the exception of the 23-tone test.

    As for the test setup we are running a TIMS test set to a 66 block which connects to the card/cage via 60 pin telco cable. We've never quantified our circuits by THD before, but maybe I should look into it...

    On the card itself after passing through the op-amp circuits it goes to a AD1938 codec and to the ADAU1442 for processing.

    Could the internal filters of the DSP be causing the bad harmonics in the Intermod distortion test?

    Thanks for responding to my post.

Children
No Data