Hi
AD8541 revG datasheet say
Regarding about Large Signal Voltage Gain
Avo= 100V/mV @ Vs=2.7V, 3.0V
but Avo=20V/mV @ Vs=5.0V
Load is 100Kohm, so these are not a big difference, I think.
Could I see the "Avo vs Vs" feature?
Regards
moto
Dear Anna
I beleve in ADI datasheet.
This Avo feature is changed by Vs drastic.
So I would like to know changing point.
Dear Anna Datasheet say "The AD8541/AD8542/AD8544 are optimized to maintain high gains at lower supply voltages, making them useful for active filters and gain stages. " Does it control by the switch? Regards moto