Spice Opamp model noise

Hi,

I downloaded the spice model for AD8676 and tried to simulate the noise in LTspice.

My circuit is really simple (see attached pdf).

The opamp is connected as a unity gain buffer. The only resistor is an Rs from the positive input to ground.

I am using +/-15V supplies (I also checked with +/-5V supplies and get same results).

I then swept the Rs value from 1 to 1G and plotted V(onoise) at 1kHz.

From that I find:

Vn=21.3nV/rHz

In=21.5fA/rHz

The datasheet says

Vn = 2.8nV/rHz

In = 300fA/rHz

So the simulated voltage noise seems to be ~10x too high and current noise is 15x too low.

Am I doing something wrong or is there a problem with the model for AD8676?

Thanks,

John

Opamp_noise.pdf
Parents Reply Children
No Data