AD8145 doesn't work exactly.

Dear Sir/Madam,

I need your help.

My schematic:

cf5b8619e13a6629748eb9fcb37b1341.bin

VREF is provided directly by AD5765. I set the common mode voltage of Vin to 0.5 V and the differential mode voltage to 1.0 V.

AD5765's output voltage is set to 0 V.  Than I measure the voltage of AD8145's REF pin. However, it's not 0 V(Of course, AD5765 doesn't work exactly now). The voltage on REF pin has following features:

Its frequency is the same as Vin;

The following pictures show how its Vp-p  varies with frequency:

ddcb67b663c8130f42f55ea6aa07677c.bin

58866f4eb63dcf28941b89e8d64e5890.bin

My question is that why REF pin of AD8145 is not 0 V ?

Parents Reply Children
No Data