Post Go back to editing

a couple of question for AD8260

Dear Sir/Madam,

I have a couple of question for your AD8260.

1)

I will just use only the high current driver part.

Not use VGA/PreAMP and VMID buffer parts.

If so, how should I connect the NOT USING PIN,  GND or OPEN or Pull-up high level?

And please give me the good comment for such way? Can I use only high current driver part?

2)

Can I use by 5V single ended power supply for the high currnet part?

If so yes, what is the output current? How should think it?

On your data sheet. I can see RLOAD = 1 Ω, VIN = ±0.5 V +/-310mA only ,I cannot find the case of single end input.

Our application is radio device.

AD8260 get the diff-signal 1Vp-p from AD9762 DAC and take the signal to next LPF for transmit by antenna.

AD9762 get the 3MHz FSK signal from front device. So I use the signal 1MHz to 4MHz on AD8260.

If you have an another good device for this case, please recommend it to me?

I need around 0.3W the outout power from driver.

Thanks Kaos

Parents
  • Hi Kris,

    Thanks for your reply.

    I just confirmed your recommended 4-devices.

    AD8390

    The diff. output doesnt fit for our next stage.

    AD8397

    The peak AC current is smaller than AD8018 we are using at present.

    AD8016

    The output 400mA min - 600mA typ sounds good, but we dont have negative power source.

    AD8018

    We  are using this device but the output current is insufficiency it is 350mA min.

    We would like to replace this to another high current output device.

    How do you think about this using the one part of AD8260? Not recommend?

    We will use it (but not fix) as the current buffer amp gain=1.

    And I will put the another question sled for SSM2211 audio amp.

    It also study for this application.

    Thanks Kaos 

Reply
  • Hi Kris,

    Thanks for your reply.

    I just confirmed your recommended 4-devices.

    AD8390

    The diff. output doesnt fit for our next stage.

    AD8397

    The peak AC current is smaller than AD8018 we are using at present.

    AD8016

    The output 400mA min - 600mA typ sounds good, but we dont have negative power source.

    AD8018

    We  are using this device but the output current is insufficiency it is 350mA min.

    We would like to replace this to another high current output device.

    How do you think about this using the one part of AD8260? Not recommend?

    We will use it (but not fix) as the current buffer amp gain=1.

    And I will put the another question sled for SSM2211 audio amp.

    It also study for this application.

    Thanks Kaos 

Children
No Data