About AD8512

Our customers have to consider the use of AD8512.

Circuit uses the p16 Figure 50 of the data sheet.
However, waveform, such as Figure 52 is not output in the simulation of LTSpice.

Do you know that do not cause the waveform of the same?

Pink waveform si OUT_B
Green waveform is input VIN

It is used to download from the homepage of ADI's Spice model of the AD8512.

Regards,
Yuji