Hello,
I am DFAE from Phoenix technologies in Israel.
Is the ADCMP572/ADCMP573 may be operated from VCC= 2.5V
Regards,
Meir
Hi meir,
The ADCMP572/3 is only guaranteed to work for supply voltages from 3.1 to 5.4V for both input and output stages. The specifications in the datasheet are shown below:
Please let me know if you need anything else.
Thanks!
Kris
Hi Kris,
sorry to bring back an already answered topic, but I had the same exact question as the original poster and I would like to point to Figure 23 on page 12 of the datasheet of ADCMP572/573, which clearly shows a case of Vcco=2.5V.
Is that figure a mistake on the datasheet?
As a side note, ADCMP580/581/582, a very similar device made from the same fabrication process (with dual power rails), does allow a Vcco of 2.5V.
Best regards,
Dimitris
Hi Dimitris,
Thank you for pointing that out. I will make sure this gets back to the product owner to clarify this issue.
Thanks,
thank you very much for the reply. Please keep me in the loop if there is any feedback from the product owner.