ADCMP582 Comparator: Disable Latch Feature.

In the Rev A data sheet for the ADCMP582, there is a figure that illustrates a method for disabling the latch feature.

Here's the figure:

I plan to use this device with Vcco=+3.3V.

The LE pin is shown connected to Vcco via a 750 Ohm resistor. Since the LE pin is terminated to VTT by 50 Ohms,

I calculate the voltage at the LE pin will be +1.4V.

The complimentary LE input, I'll call it LEBAR is connected to VTT, giving LEBAR=+1.3V.

So we see that LE is HIGH and LEBAR is LOW. This should disable the latch feature. Good.

My question is this: Is Figure 23 incorrect?

I ask this because the minimum Latch Enable Input Differential Voltage given in Table 1 for the ADCMP582 in PECL mode

is 200mV. The circuit of Figure 23 produces a differential of 100mV.

There is no discussion of Figure 23 in the data sheet.

Cheers,

David