We have had success in building an amplification circuit with the OP497 G class amplifier. Our application is amplifying a very low current DC input signal from a photodiode which will be charge integrated after the output in a CAEN V792N QDC card.
We are looking for something a little smaller in size to fit on our amp boards. We still need low input bias current and a quad op-amp package with 14 pins. Do you have an amplifier like the OP497, or a smaller version of the OP497? The approximate dimensions are 4mm x 8mm (package only, without pins). For reference, we need something the same size as the LT1817S amplifier:
http://cds.linear.com/docs/en/datasheet/181567fb.pdf
(See page 19 for dimensions on "S-package").
Thanks!
Hi Kole,
You could take a look at the AD8669 or the AD8659. The AD8669 is more similar to the OP497, so i would check that out first. The package you are looking for is the 14-lead SOIC-N.
Please let me know if these amplifiers will cater to the needs of your applications.
Kris