Post Go back to editing

Can ADA4000-4 work on +-18V power supply?

Hello,

I am searching one kind of opamp to work on +-18V. ADA4000-4  may be the choice as the datasheet said that "±4 V to ±18 V operation". However, I also found in the datasheet that the maximum supply voltage is "±18 V".

So my question is that could I use the ADA4000-4 in the system with ±18 V power supply? If not, any good recommendation of opamp (those with similar performance as ADA4000-4 are OK)

Thank you very much!

Billy

Parents Reply Children
No Data