Post Go back to editing

How to unleash the outputs of operational amplifiers are connected to a common load?

Used operational amplifiers AD8534 and AD8532.

Parents
  • Hi, Phil. In the figure, part of the circuit. Maybe there is nothing wrong with the signals from the outputs of the operational amplifiers can not simultaneously appear at the output due to a temporary demarcation work DACs. But I am concerned about their influence in the static mode. In the static mode, the output voltage is equal to 5V. The main thing for me - the absence of a possible short circuit. When designing a circuit I made a mistake and did not notice that connect the output of the operational amplifiers is now trying to address this shortcoming.

Reply
  • Hi, Phil. In the figure, part of the circuit. Maybe there is nothing wrong with the signals from the outputs of the operational amplifiers can not simultaneously appear at the output due to a temporary demarcation work DACs. But I am concerned about their influence in the static mode. In the static mode, the output voltage is equal to 5V. The main thing for me - the absence of a possible short circuit. When designing a circuit I made a mistake and did not notice that connect the output of the operational amplifiers is now trying to address this shortcoming.

Children
No Data