Post Go back to editing

Whats the best Inamp for high speed current sensing?

Hi all,

I am working on a device to measure the current of a supply in real time.  The purpose of this, is to help with software development of ultra-low power 'always on' devices to be more efficient.  The biggest market for this currently is IoT.

I want to have both speed and accuracy from an amplifier and I have therefore discarded all of the purpose made current sense amplifiers as they don't provide sufficient bandwidth for my application.

The specifications required are as follows:

  • The highest voltage supply to be measured will be +5V to 0V. and the maximum current will be 1A.  I will most likely use a 50mohm shut resistor, giving the maximum differential voltage of 50mV.  I would also like for it to be accurate to the 100'suA scale, meaning that the differential voltage accuracy needs to be < 10uV (although I may use a 0.1ohm resistor for the lower scale). 
  • I need a high bandwidth across the gain range as I plan to use a 500ksps ADC to digitize the analog voltage, although will most likely be using 100-150ksps.
  • It needs to have very good common mode rejection ratio.
  • It needs to have the voltage offset as low as possible to get the best accuracy.
  • Adjustable gain is a must ideally from an external resistor, that I will drive from a digital Pot.

I have been looking at the AD8220 for a rail to rail inamp, or the AD8221 which appears to be a better device for me, but will require a dual supply to get the full swing.

Can anyone suggest any better suited iamps that I have missed, or do these 2 seem the best suited for this application?

Any support will be very much appreciated.

Many Thanks Ian.

Parents
  • Have you looked at the AD8130? it's intended as  a differential line receiver, but is very fast ( a faster variant of the AD8420 mentioned above).  It uses indirect current feedback, so for example you can refer the output signal to mid supply for bipolar input to a differential ADC. It only uses a single gain resistor, so it is possible to change the gain without the CMRR issues. and it works nearly rail to rail, so no issues with the "hexagon".

Reply
  • Have you looked at the AD8130? it's intended as  a differential line receiver, but is very fast ( a faster variant of the AD8420 mentioned above).  It uses indirect current feedback, so for example you can refer the output signal to mid supply for bipolar input to a differential ADC. It only uses a single gain resistor, so it is possible to change the gain without the CMRR issues. and it works nearly rail to rail, so no issues with the "hexagon".

Children
No Data