Drop-in replacement for LM837?

    Does ADI have a form, fit, and function replacement for the LM837 in a SO-14 package?  Our applications are in low-noise audio, with + and - 12 -- 15 V rails.

     Thanks, Bob

Parents
  • 0
    •  Analog Employees 
    on Oct 9, 2015 5:12 AM over 5 years ago

    Hi Bob,

    Sorry to hear that. You can also look at ADTL084, with respect to LM837, they almost have the same specs. with THD+N with the value of 0.001% which is a little lower than LM837 THD with a value of 0.0015. And it also works within the range of your requirement on rail-to-rail voltage of +/-12 to 15V.  As for the price, ADTL084 cost $0.92 per 1000 pcs.

    Chard

Reply
  • 0
    •  Analog Employees 
    on Oct 9, 2015 5:12 AM over 5 years ago

    Hi Bob,

    Sorry to hear that. You can also look at ADTL084, with respect to LM837, they almost have the same specs. with THD+N with the value of 0.001% which is a little lower than LM837 THD with a value of 0.0015. And it also works within the range of your requirement on rail-to-rail voltage of +/-12 to 15V.  As for the price, ADTL084 cost $0.92 per 1000 pcs.

    Chard

Children
No Data