Post Go back to editing

AD204 OSCILLATOR DRIVE INPUT

Hi,all

OSCILLATOR DRIVE INPUT SPECIFICATIONS @ AD204 datasheet,

Input Voltage 15 V p-p Nominal

Input Frequency 25 kHz Nominal

What is the margin tolerance for each spec.?

+/-?%

What is the ABSOLUTE MAXIMUM RATINGS ?

Best Regards,

sss

Parents
  • Hi sss,

    According to the product owner of this part, the AD204 was designed many years ago and the datasheets did not include Absolute Maximum ratings.

    He also added that knowing the AD204 module also generates internal voltages from the Oscillator Drive input, you should be safe operating with a +/-5% tolerance on the Oscillator Drive signal.

    The Oscillator Drive Input on the AD204 module was designed to be driven from our AD246 clock driver module which has enough drive current to power multiple AD204 modules.

    The frequency of the AD246 clock driver module is tested at the factory to be within 25KHz +/-10%.

    I hope this helps.

    Best regards,

    Emman

Reply
  • Hi sss,

    According to the product owner of this part, the AD204 was designed many years ago and the datasheets did not include Absolute Maximum ratings.

    He also added that knowing the AD204 module also generates internal voltages from the Oscillator Drive input, you should be safe operating with a +/-5% tolerance on the Oscillator Drive signal.

    The Oscillator Drive Input on the AD204 module was designed to be driven from our AD246 clock driver module which has enough drive current to power multiple AD204 modules.

    The frequency of the AD246 clock driver module is tested at the factory to be within 25KHz +/-10%.

    I hope this helps.

    Best regards,

    Emman

Children
No Data