Post Go back to editing

ADA4941-1 opened input signal

Hello

I am considering Sallen-Key, Low-Pass Filter like figure 54 on the datasheet.

There is a situation that the input is opened.

Then the output would be unstable.

Should I put termination resistor?

If yes, which value can I use?

There is a little oscillation at output because of load capacitance.

How can I compensate it?

Regards,

Parents
  • FormerMember
    0 FormerMember
on Mar 10, 2016 6:15 PM

power-man-san,

  What frequency?  What amplitude?

How much load capacitance?

I would suspect pc board layout first.

For a test, change the 1.69k resistor to 100 ohms.

Harry

Reply
  • FormerMember
    0 FormerMember
on Mar 10, 2016 6:15 PM

power-man-san,

  What frequency?  What amplitude?

How much load capacitance?

I would suspect pc board layout first.

For a test, change the 1.69k resistor to 100 ohms.

Harry

Children
No Data