Post Go back to editing

AD8036 Clamping Amplifier Accuracy over Temperature

The AD8036 has typical input offset and offset tempco specified as 2 mV and 10uV/C, respectively.  And the clamp accuracy is 3 mV typical.  Is there a tempco spec available for the clamp accuracy?  Also, is there a hysteresis spec for the clamp performance?  My application is for DC and low frequency signals of less than 1 kHz.

Thanks,

Steve

Parents
  • Hello Steve,

    Apologies for delayed response. For your question, I'm sorry to say that we don't have any available data for clamp performance over temperature. The hysteresis was also not shown on any plot in the datasheet but the input clamping operation including the comparator's performace was discussed in details on the clamping operation section in the datasheet on page 16.

    Regards,

    Phil

Reply
  • Hello Steve,

    Apologies for delayed response. For your question, I'm sorry to say that we don't have any available data for clamp performance over temperature. The hysteresis was also not shown on any plot in the datasheet but the input clamping operation including the comparator's performace was discussed in details on the clamping operation section in the datasheet on page 16.

    Regards,

    Phil

Children
No Data